SLUSEJ1 December 2021 TPSM8D6C24
PRODUCTION DATA
The output-voltage ripple is the second criterion for output capacitor selection. Use Equation 15 to calculate the minimum output capacitance required to meet the output-voltage ripple specification.
In this case, the target maximum output-voltage ripple is 20 mV. Under this requirement, the minimum output capacitance for ripple is 110 µF. This capacitance value is smaller than the output capacitance required for the transient response, so select the output capacitance value based on the transient requirement. Considering the variation and derating of capacitance, in this design, two 470-µF low-ESR tantalum polymer bulk capacitors and four 47-µF ceramic capacitors were selected to meet the transient specification with sufficient margin. Therefore the selected nominal COUT is equal to 1128 µF.
With the output capacitance value selected the ESR must be considered. This is an important consideration in this example because it uses mixed output capacitor types. First use Equation 16 to calculate the maximum allowable impedance for the output capacitor bank at the switching frequency to meet the output voltage ripple specification. Equation 16 indicates the output capacitor bank impedance should be less than 2.1 mΩ. The impedance of the ceramic capacitors is calculated with Equation 17 and the impedance of the bulk capacitor is calculated with Equation 18. The result from Equation 18 shows the impedance of the bulk capacitor at the switching frequency is dominated by its ESR. Equation 19 calculates the total output impedance of the output capacitor bank at the switching frequency to be 1.2 mΩ which meets the 2.1 mΩ requirement.