To begin the design process, determine the following:
- Input voltage range
- Use the supply voltage of the device that is
driving the TXG802x device to
determine the input voltage range. For a valid logic-high, the value
must exceed the positive-going input-threshold voltage
(VT+) of the input port. For a valid logic low the
value must be less than the negative-going input-threshold voltage
(VT-) of the input port.
- Output voltage range
- Use the supply voltage of the device that the TXG802x device is driving to
determine the output voltage range.