JAJSAX7E April 2008 – May 2016 LM2758
PRODUCTION DATA.
The LM2758 is an adaptive 1× and 1.5× CMOS charge pump, optimized for driving flash LEDs in camera phones and other portable applications. It provides a constant current of 500 mA (typical) for flash mode and 107 mA (typical) for torch mode with RSET = 20 kΩ. These current can change (see Setting LED Currents).
There are four modes of operation for LM2758: the flash mode, torch mode, indicator mode, and shutdown mode (see Table 1). Torch and flash modes sink a constant DC current while indicator mode operates in pulsating DC at 1/32 positive duty cycle with same current magnitude as torch mode. The LED is driven from CPOUT and connected to the current sink. LED drive current mode is programmed by connecting a resistor, RSET, to the current set pin, ISET. The LM2758 device also controls CPOUT with variable gain (1× or 1.5×) and adjustable impedance (ROUT) to provide an output voltage that would account for LED forward voltage drop and headroom for the current sink to drive desired current through LED.
The input to the 1×/1.5× charge pump is connected to the VIN pin, and the loosely regulated output of the charge pump is connected to the CPOUT pin. In 1× mode, as long as the input voltage is less than 4.7 V, the output voltage is approximately equal to the input voltage. When input voltage is over 4.7 V the output voltage is regulated to 4.7 V. In 1.5× mode, the output voltage is always less than or equal to 4.7 V over entire input voltage range.
The gain of the charge pump is selected depending on the headroom voltage across the current sink of LM2758. When headroom voltage VLED– (at the LED pin) drops below 300 mV (typical) the charge-pump gain transition happens from 1× to 1.5× to maintain current regulation across the LED. Once the charge pump transition to a higher gain, it remains at that gain for as long as the device remains enabled. Shutting down and then re-enabling the device resets the gain mode to the minimum gain required to maintain the load.
The LM2758 contains internal soft-start circuitry to limit inrush currents when the part is enabled. Soft start is implemented internally with a controlled turnon of the internal voltage reference.
The LM2758 charge pump contains current limit protection circuitry that protects the device during VOUT fault conditions where excessive current is drawn. Output current is limited to 1.2 A typically.
Flash time-out protection circuitry disables the current sinks when the signal on EN1 and EN2 is held high for more than 814 msec (typical). This prevents the device from self-heating due to the high power dissipation during flash conditions. During the time-out condition, voltage is still present on CPOUT but the current sinks are shut off, resulting in no current through the flash LED. When the device goes into a time-out condition, placing a logic low signal on EN1 and EN2 resets the timeout; a subsequent logic high signal on EN1 or EN2 returns the device to normal operation.
The current through the LED can be set by connecting an appropriately sized resistor RSET between the ISET pin of the LM2758 and GND.
The LED current in torch mode is approximately 1639 times greater than the current of ISET, while the LED current in flash mode is approximately 7650 times of the same ISET current. The feedback loop of an internal amplifier sets the voltage of the ISET pin to 1.3 V (typical). The statements above are simplified in Equation 1:
The maximum recommended current through LED is 500 mA in torch mode / 700 mA in flash mode.
NOTE
If the ISET for torch mode setting at 500 mA, the flash mode would be over 700 mA (maximum). See Figure 6. Using the device in conditions where the junction temperature might rise above the rated maximum requires that the operating ranges and/or conditions be de-rated. The printed circuit board also must be carefully laid out to account for high thermal dissipation in the part.
Figure 7. Analog Brightness Control
The current through the LED can be varied dynamically by changing the ISET current. Figure 7 shows the circuit. The current though the LED can be calculated with Equation 2:

Internal thermal protection circuitry disables the LM2758 when the junction temperature exceeds 150°C (typical). This feature protects the device from being damaged by high die temperatures that might otherwise result from excessive power dissipation. The device recovers and operates normally when the junction temperature falls below 140°C (typical). It is important that the board layout provide good thermal conduction to keep the junction temperature within the specified operating ratings.
There are four modes of operation for LM2758: the flash mode, torch mode, indicator mode and shutdown mode (see Table 1). Torch and flash modes sink a constant DC current while indicator mode operates in pulsating DC at 1/32 positive duty cycle with same current magnitude as torch mode.
The LM2758 has two logic pins, EN1 and EN2. There is a 500-kΩ (typical) pulldown resistor connected from EN1 to GND and from EN2 to GND. The operating modes of the part function according to Table 1:
| EN1 | EN2 | MODE |
|---|---|---|
| 0 | 0 | Shutdown |
| 1 | 0 | Indicator |
| 0 | 1 | Torch |
| 1 | 1 | Flash |