JAJSIB3D August 2017 – February 2021 THS4561
PRODUCTION DATA
The most important elements to the closed-loop performance are the open-loop gain and open-loop output impedance. Figure 10-1 shows the simulated differential open-loop gain and phase from the differential inputs to the differential outputs with no load and with a 100-Ω load. Operating with no load removes any effect introduced by the open-loop output impedance to a finite load. Figure 10-2 shows the simulated differential open-loop output impedance.
This open-loop output impedance combines with the load to shift the apparent open-loop gain and phase to the output pins when the load changes. The rail-to-rail output stage shows a very high impedance at low frequencies that reduces with frequency to a lower midrange value and then peaks again at higher frequencies. The maximum value at low frequencies is set by the common-mode sensing resistors to be a 6-kΩ dc value (see Section 9.2.) This high impedance at a low frequency is significantly reduced in closed-loop operation by the loop gain, as shown in the closed-loop output impedance of Figure 7-43. Figure 10-1 compares the no load AOL gain to the AOL gain driving a 100-Ω load that shows the effect of the output impedance. The heavier loads pull the AOL gain down faster to lower crossovers with more phase shift at the lower frequencies.
The much faster phase rolloff for the 100-Ω differential load explains the greater peaked response illustrated in Figure 7-4 and Figure 7-18 when the load decreases. This same effect happens for the RC loads common with converter interface designs. Use the TINA-TI™ model to verify loop phase margin in any design.