JAJSME8C July 2021 – June 2022 TMP126
PRODUCTION DATA
Bit 9 of the command word is the auto-increment bit.
Setting this bit to 1 will cause the address pointer of the TMP126 to increment by after every word of data on a read or write transaction. If the bit is set to 0, the address pointer is not incremented and reads/writes will continue to only apply the Sub-Address specified in the command word.