• DWK|14
  • DW|16
サーマルパッド・メカニカル・データ
発注情報

Layout Example

Figure 42 shows a 2-layer PCB layout example with the signals and key components labeled for SOIC-16 DW package. SOIC-14 DW package has Pin 12 and Pin 13 removed. For more detailed information, please refer to the UCC21540EVM design - "Using the UCC21540EVM - TI"

UCC21540 UCC21541 fig41_lusc9.gifFigure 42. Layout Example

Figure 43 and Figure 44 shows top and bottom layer traces and copper.

NOTE

There are no PCB traces or copper between the primary and secondary side, which ensures isolation performance.

PCB traces between the high-side and low-side gate drivers in the output stage are increased to maximize the creepage distance for high-voltage operation, which will also minimize cross-talk between the switching node VSSA (SW), where high dv/dt may exist, and the low-side gate drive due to the parasitic capacitance coupling.

UCC21540 UCC21541 fig42_lusc9.gif
Figure 43. Top Layer Traces and Copper
UCC21540 UCC21541 fig43_lusc9.gif
Figure 44. Bottom Layer Traces and Copper (Flipped)

Figure 45 and Figure 46 are 3-D layout pictures with top view and bottom views.

NOTE

The location of the PCB cutout between the primary side and secondary sides, which ensures isolation performance.

UCC21540 UCC21541 fig44_lusc9.gif
Figure 45. 3-D PCB Top View
UCC21540 UCC21541 fig45_lusc9.gif
Figure 46. 3-D PCB Bottom View