Gate Driver Output Resistor

The external gate driver resistors, RON/ROFF, are used to:

  • Limit ringing caused by parasitic inductances/capacitances.
  • Limit ringing caused by high voltage/current switching dv/dt, di/dt, and body-diode reverse recovery.
  • Fine-tune gate drive strength, i.e. peak sink and source current to optimize the switching loss.
  • Reduce electromagnetic interference (EMI).

As mentioned in Output Stage, the UCC2154x has a pull-up structure with a P-channel MOSFET and an additional pull-up N-channel MOSFET in parallel. The combined peak source current is 4 A. Therefore, the peak source current can be predicted with:

Equation 3. UCC21540 UCC21541 eq3_slusck0.gif
Equation 4. UCC21540 UCC21541 eq4_slusck0.gif

where

  • RON: External turn-on resistance.
  • RGFET_INT: Power transistor internal gate resistance, found in the power transistor datasheet.
  • IO+ = Peak source current – The minimum value between 4 A, the gate driver peak source current, and the calculated value based on the gate drive loop resistance.

In this example:

Equation 5. UCC21540 UCC21541 eq5_slusck0.gif
Equation 6. UCC21540 UCC21541 eq6_slusck0.gif

Therefore, the high-side and low-side peak source current is 2.3 A and 2.5 A respectively. Similarly, the peak sink current can be calculated with:

Equation 7. UCC21540 UCC21541 eq7_slusck0.gif
Equation 8. UCC21540 UCC21541 eq8_slusck0.gif

where

  • ROFF: External turn-off resistance, ROFF=0 in this example;
  • VGDF: The anti-parallel diode forward voltage drop which is in series with ROFF. The diode in this example is an MSS1P4.
  • IO-: Peak sink current – the minimum value between 6 A, the gate driver peak sink current, and the calculated value based on the gate drive loop resistance.

In this example,

Equation 9. UCC21540 UCC21541 eq9_slusck0.gif
Equation 10. UCC21540 UCC21541 eq10_slusck0.gif

Therefore, the high-side and low-side peak sink current is 5.0 A and 5.4A respectively.

Importantly, the estimated peak current is also influenced by PCB layout and load capacitance. Parasitic inductance in the gate driver loop can slow down the peak gate drive current and introduce overshoot and undershoot. Therefore, it is strongly recommended that the gate driver loop should be minimized. On the other hand, the peak source/sink current is dominated by loop parasitics when the load capacitance (CISS) of the power transistor is very small (typically less than 1 nF), because the rising and falling time is too small and close to the parasitic ringing period.