DLPU082B August 2021 – August 2022 DLPC7540
Set Image Algorithm Enable | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Chroma Transient Improvement Enable bit 0: Chroma Transient Improvement Enable Bit |
Byte 1 |
Gamma Correction Enable bit 0: Gamma Correction Enable Bit |
Byte 2 |
Color Coordinate Adjustment Enable bit 0: Color Coordinate Adjustment Enable Bit |
Byte 3 |
Brilliant Color Enable bit 0: Brilliant Color Enable Bit |
Byte 4 |
White Point Correction Enable bit 0: White Point Correction Enable Bit |
Byte 5 |
Dynamic Black Enable bit 0: Dynamic Black Enable Bit |
Byte 6 |
HDR Enable bit 0: HDR Enable Bit |
Sets enable flag for all Image Algorithms. 0 = Disable 1 = Enable Chroma Transient Improvement : This function enables/disables the Chroma Transient Improvement (CTI) function which filters the 4 : 4 : 4 sampled, chrominance (Cr and Cb) data on the B and C data channels. The chroma transient functions performs band pass filtering (supports two center frequencies) and median filtering for ringing minimization. It performs limiting and coring functions for the filtered output. Gamma Correction : This function enables/disables the Gamma Correction function which implements the removal of gamma transfer function applied at the source, via table lookup process called de-gamma. When enabled, perform de-gamma translation of the 10-bit RGB input to the common 12-bit floating point (S0M8E4) RGB output. When disabled, the full 10 bits of each data input to the Gamma Correction function are zero padded and MSB-aligned to 12-bits and passed through unmodified. Color Coordinate Adjustment : This function enables/disables the Spatially Adaptive Seven Primaries Color Correction Function Enable. When Disable forces 3x3 CSC (Color Space Conversion) with identity. Brilliant Color : This function enables/disables the BrilliantColor technology, Brilliant Color uses up to five colors, instead of just the three primary colors, red, green and blue, to improve color accuracy and brightens of secondary colors. This results in a new level of color performance that increases the brightness of the colors. White Point Correction : This function enables/disables the White Point Correction, typically used on LED type illumination systems. Sometimes due to increase in LED operating temperature or LED aging the LEDs output wavelentgh drifts, therefore white point of the system shifts. This algorithm using active light sensor feedback and factory calibrated values help maintaing white point of the system. Dynamic Black : Dynamic Black (DB) is an algorithm that reduces the amount of light reaching the projection path by means of LED output power through current control and compensates for reduced light by gaining up the RGB signals. HDR : High Dynamic Range (HDR) is an algorithm that maps wider brightness and color range of HDR source to the projector display range. HDR is affected by several factors such as illimuniation characterstics, duty cycle distribution and current running sequence. A valid HDR source should be set by HDR_SetHdrSourceConfiguration() before enabling HDR processing. Note: Chroma Transient Improvement is applicable to Analog SDTV sources only. DLPC6540 controller doesn't support Analog sources. Even if enabled on DLPC6540 controller, there is no changes in the displayed image when enabled. |
Get Image Algorithm Enable | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns enable flag for all Image Algorithms '0' - Disabled or algorithm feature not available. '1' - Enabled |
Set Image Brightness | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Brightness Adjustment Range = -256.00 to 255.75 with step size .25 Format = s14.2 |
The brightness control provides the ability to add or subtract a fixed bias from each of the input channels. This may be used to remove any inherent offsets and/or adjust the brightness level. The brightness coefficients are signed, 11-bit (s8.2), 2's complement values between -256 and 255.75, inclusive. Brightness Control is used after Color Space Conversion. |
Get Image Brightness | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns Image Brightness Level. |
Set Image Contrast | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Contrast (%) Range = 0 to 200 with step size 1 |
Sets Image Contrast in percentage. Each contrast byte controls the gain applied to the input image data for a given data channel. The contrast gain has a range from 0 to 200 (0% to 200%) with 100 (100%) being nominal (default). |
Get Image Contrast | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns Image Contrast in percentage. |
Set Image Hue And Color Control | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Hue Adjustment Angle (degrees) Range = -45 to 45 with step size 1 |
Bytes 1-2 |
Color Control Gain (%) Range = 0 to 200 with step size 1 |
Sets Image Hue Adjustment angle in degrees and Color Control Gain in percentage. |
Get Image Hue And Color Control | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns Image Hue Adjustment angle in degrees and Color Control Gain in percentage. |
Set Image Sharpness | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Sharpness value to apply. Range = 0 to 31 with step size 1 |
Configures the sharpness filter. A value of 0 is the least sharp (smoothest), while a value of 31 is the sharpest. This filter is in the back end of the data path, so both video and graphics are affected. TI recommends that the sharpness filters be disabled (sharpness=16) for graphics sources. |
Get Image Sharpness | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns the current sharpness value |
Set Image RGB Offset | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Red channel offset setting. Range = -256.00 to 255.75 with step size .25 Format = s14.2 |
Bytes 2-3 |
Green channel offset setting. Range = -256.00 to 255.75 with step size .25 Format = s14.2 |
Bytes 4-5 |
Blue channel offset setting. Range = -256.00 to 255.75 with step size .25 Format = s14.2 |
Offsets the levels of the RGB channels at a point in the data path after the following image processing functions have been applied - source offset, contrast, RGB Gain, Brightness and Color Space Conversion (including Hue and Color Adjustment). |
Get Image RGB Offset | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns Red, Green and Blue channel offset settings. |
Set Image RGB Gain | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Red channel gain setting. Range = 0 to 200 with step size 1 |
Bytes 2-3 |
Green channel gain setting. Range = 0 to 200 with step size 1 |
Bytes 4-5 |
Blue channel gain setting. Range = 0 to 200 with step size 1 |
Adjusts individual R, G and B gains of the source image. Gain is specified as a percentage from 0% - 200%, with 100% being nominal (no gain change). 0% will zero out the channel. This function adjusts R, G and B gains by altering the Color Space Conversion (CSC) coefficients. This function is only applicable to RGB sources. |
Get Image RGB Gain | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns gain setting for Red, Green and Blue color channels in percentage. |
Set CSC Table | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Index of the pre-defined CSC table in flash. Range = 0 to 7 with step size 1 0 = Table Fullrange Rgb 1 = Table Bt601 Yuv Videodecoder 2 = Table Fullrange Yuv1 3 = Table Offset Rgb 4 = Table Bt601 Offset Yuv 5 = Table Fullrange Yuv 6 = Table Bt709 Offset Yuv 7 = Table Smpte 240m 8 = Table Bt2020 9 = Maxtable |
Sets the Color Space Conversion Matrix with one of the CSC tables stored in flash. |
Get CSC Table | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Gets the index of the Color Space Conversion Matrix that is currently cofigured for use. |
Set Image CCA Coordinates | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Original Coordinate Red x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 2-3 |
Original Coordinate Red y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 4-5 |
Original Coordinate Red Lum Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 6-7 |
Original Coordinate Green x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 8-9 |
Original Coordinate Green y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 10-11 |
Original Coordinate Green Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 12-13 |
Original Coordinate Blue x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 14-15 |
Original Coordinate Blue y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 16-17 |
Original Coordinate Blue Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 18-19 |
Original Coordinate White x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 20-21 |
Original Coordinate White y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 22-23 |
Original Coordinate White Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 24-25 |
Original Coordinate C1 x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 26-27 |
Original Coordinate C1 y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 28-29 |
Original Coordinate C1 Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 30-31 |
Original Coordinate C2 x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 32-33 |
Original Coordinate C2 y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 34-35 |
Original Coordinate C2 Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 36-37 |
Original Coordinate DRA A x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 38-39 |
Original Coordinate DRA A y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 40-41 |
Original Coordinate DRA A Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 42-43 |
Original Coordinate DRA B x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 44-45 |
Original Coordinate DRA B y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 46-47 |
Original Coordinate DRA B Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 48-49 |
Original Coordinate DRA C x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 50-51 |
Original Coordinate DRA C y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 52-53 |
Original Coordinate DRA C Luminance Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 54-55 |
Target Coordinate Red x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 56-57 |
Target Coordinate Red y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 58-59 |
Target Coordinate Red Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 60-61 |
Target Coordinate Green x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 62-63 |
Target Coordinate Green y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 64-65 |
Target Coordinate Green Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 66-67 |
Target Coordinate Blue x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 68-69 |
Target Coordinate Blue y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 70-71 |
Target Coordinate Blue Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 72-73 |
Target Coordinate Cyan x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 74-75 |
Target Coordinate Cyan y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 76-77 |
Target Coordinate Cyan Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 78-79 |
Target Coordinate Magenta x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 80-81 |
Target Coordinate Magenta y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 82-83 |
Target Coordinate Magenta Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 84-85 |
Target Coordinate Yellow x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 86-87 |
Target Coordinate Yellow y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 88-89 |
Target Coordinate Yellow Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 90-91 |
Target Coordinate White x Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 92-93 |
Target Coordinate White y Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
Bytes 94-95 |
Target Coordinate White Gain Range = 0.0 to 1.99996948242 with step size 0.00003051757 Format = u1.15 |
This Command allows independent adjustment of the primary, secondary and white coordinates. Note: This call will override any CCA settings performed by prior calls. |
Get Image CCA Coordinates | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns the current color coordinate configuration. |
Set Image HSG | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
HSG Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 2-3 |
HSG Red Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 4-5 |
HSG Red Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 6-7 |
HSG Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 8-9 |
HSG Green Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 10-11 |
HSG Green Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 12-13 |
HSG Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 14-15 |
HSG Blue Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 16-17 |
HSG Blue Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 18-19 |
HSG Cyan Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 20-21 |
HSG Cyan Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 22-23 |
HSG Cyan Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 24-25 |
HSG Magenta Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 26-27 |
HSG Magenta Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 28-29 |
HSG Magenta Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 30-31 |
HSG Yellow Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 32-33 |
HSG Yellow Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 34-35 |
HSG Yellow Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 36-37 |
HSG White Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 38-39 |
HSG White Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 40-41 |
HSG White Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
This command applies the given Hue, Saturation and Gain values for all colors. It does not affect colors having a gain of zero. Note: This call will override any CCA settings performed by prior calls. |
Get Image HSG | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
This command returns the currently applied Hue, Saturation and Gain values for all the colors. If Gain for a color is zero then the HSG is not applied on the color. |
Set Image Gamma LUT | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Gamma look-up table to load. |
This command loads the specified Gamma look-up table into memory from flash. A single load is accomplished by loading data for red, green and blue look-up tables. |
Get Image Gamma LUT | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns the table number of the Gamma look-up table currently loaded in memory. |
Set Image Gamma Curve Shift | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Red Gamma curve shift. Range = -128 to 127 with step size 1 |
Byte 1 |
Green Gamma curve shift. Range = -128 to 127 with step size 1 |
Byte 2 |
Blue Gamma curve shift. Range = -128 to 127 with step size 1 |
Byte 3 |
Broadcasted shift to Gamma curves of all color. Range = -128 to 127 with step size 1 |
Used to specify the shifts in the Gamma curve of Red, Green and Blue. A left shift is a positive offset and a right shift is a negative offset. The effective brightness is increased with a left shift and decreased with a right shift. |
Get Image Gamma Curve Shift | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns Image Gamma Shift for red, green and blue as well as shift to be broadcasted to all colors |
Set Img White Peaking Factor | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Amount of white processing. Range 0 to 10). |
Get Img White Peaking Factor | |
---|---|
Data returned is in the same format as the Write Parameter(s). |
Set XPR Filter Strength Command | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Filter Strength setting determines how much of high frequency content is filtered out. Valid range 0-7Setting of 0 means least filtering of high frequency content (sharpest image; more flicker) Setting of 7 means most filtering of high frequency content (smoothest image; least flicker) |
Get XPR Filter Strength Command | |
---|---|
Data returned is in the same format as the Write Parameter(s). |
Set HDR Source Configuration | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Transfer Function 0 = Reserved 1 = Reserved 2 = PQ 3 = HLG |
Bytes 1-4 |
Master Display Black Level (nits) Range = 0.0000 to 10000.0 Format = u16.16 |
Bytes 5-8 |
Master Display White Level (nits) Range = 0.0000 to 10000.0 Format = u16.16 |
Bytes 9-10 |
Master Display Color Gamut Red x Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 11-12 |
Master Display Color Gamut Red y Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 13-14 |
Master Display Color Gamut Green x Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 15-16 |
Master Display Color Gamut Green y Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 17-18 |
Master Display Color Gamut Blue x Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 19-20 |
Master Display Color Gamut Blue y Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 21-22 |
Master Display Color Gamut White x Range = 0.0000 to 1.0000 Format = u1.15 |
Bytes 23-24 |
Master Display Color Gamut White y Range = 0.0000 to 1.0000 Format = u1.15 |
HDR maps wider brightness and color range of HDR sources to projector brightness and color range. The mapping requires multiple source groups and system groups to define the HDR source and projection device properties respectively. This command sets the source properties and based on this information selects nearest source group for mapping. |
Get HDR Source Configuration | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Includes the metadata information. |
Set HDR Strength Setting | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
HDR Strength Range = 0 to 10 |
Sets HDR strength which adjusts the electro-optical transfer function that is applied on the input HDR video signal. HDR strength can vary with the ambient brightness level.HDR strength is not applicable for HLG transfer function set by HDR source configuration. |
Get HDR Strength Setting | |
---|---|
Data returned is in the same format as the Write Parameter(s). |
Set System Brightness Range Setting | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-3 |
Min Brightness (nits) Range = 0.0000 to 10000.0 Format = u16.16 |
Bytes 4-7 |
Max Brightness (nits) Range = 0.0000 to 10000.0 Format = u16.16 |
Sets the system brightness range in nits. These are used in determining the appropriate EOTF and OOTF function to be applied on the HDR source. This need to set only for HDR functionality. |
Get System Brightness Range Setting | |
---|---|
Data returned is in the same format as the Write Parameter(s). |
Set Image Color Profile | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Color Profile |
Sets pre-configured Gamma table index and HSG settings as stored in the flash image. |
Set Image Point HSG | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Point 0 = Row0 Col0 1 = Row0 Col1 2 = Row0 Col2 3 = Row0 Col3 4 = Row0 Col4 5 = Row1 Col0 6 = Row1 Col1 7 = Row1 Col2 8 = Row1 Col3 9 = Row1 Col4 10 = Row2 Col0 11 = Row2 Col1 12 = Row2 Col2 13 = Row2 Col3 14 = Row2 Col4 |
Bytes 1-2 |
HSG Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 3-4 |
HSG Red Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 5-6 |
HSG Red Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 7-8 |
HSG Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 9-10 |
HSG Green Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 11-12 |
HSG Green Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 13-14 |
HSG Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 15-16 |
HSG Blue Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 17-18 |
HSG Blue Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 19-20 |
HSG Cyan Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 21-22 |
HSG Cyan Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 23-24 |
HSG Cyan Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 25-26 |
HSG Magenta Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 27-28 |
HSG Magenta Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 29-30 |
HSG Magenta Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 31-32 |
HSG Yellow Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 33-34 |
HSG Yellow Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 35-36 |
HSG Yellow Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 37-38 |
HSG White Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 39-40 |
HSG White Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 41-42 |
HSG White Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
This command applies the given hue, saturation and gain values for all colors, for a specified sample point. Point is a number 0-15 corresponding to one of the the 5 x 3 PCC sample points in raster scan order. It does not affect colors having a gain of zero. Note : This call will override any CCA settings performed by prior calls. |
Get Image Point HSG | |
---|---|
Read Parameter(s) | |
Byte | Description |
Byte 0 |
Point 0 = Row0 Col0 1 = Row0 Col1 2 = Row0 Col2 3 = Row0 Col3 4 = Row0 Col4 5 = Row1 Col0 6 = Row1 Col1 7 = Row1 Col2 8 = Row1 Col3 9 = Row1 Col4 10 = Row2 Col0 11 = Row2 Col1 12 = Row2 Col2 13 = Row2 Col3 14 = Row2 Col4 |
Return Parameter(s) | |
Byte | Description |
Bytes 0-1 |
HSG Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 2-3 |
HSG Red Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 4-5 |
HSG Red Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 6-7 |
HSG Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 8-9 |
HSG Green Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 10-11 |
HSG Green Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 12-13 |
HSG Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 14-15 |
HSG Blue Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 16-17 |
HSG Blue Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 18-19 |
HSG Cyan Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 20-21 |
HSG Cyan Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 22-23 |
HSG Cyan Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 24-25 |
HSG Magenta Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 26-27 |
HSG Magenta Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 28-29 |
HSG Magenta Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 30-31 |
HSG Yellow Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 32-33 |
HSG Yellow Saturation Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 34-35 |
HSG Yellow Hue Range = -1.0 to 1.0 with step size 0.00006103515 Format = s2.14 |
Bytes 36-37 |
HSG White Red Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 38-39 |
HSG White Green Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
Bytes 40-41 |
HSG White Blue Gain Range = 0.0 to 1.99993896485 with step size 0.00006103515 Format = s2.14 |
This command returns the currently applied hue, saturation and gain values for all the colors, for a specified sample point. Point is a number 0-15 corresponding to one of the the 5 x 3 PCC sample points in raster scan order. If gain for a color is zero then the HSG is not applied on the color. |
Set Spcc Control Points | |
---|---|
Write Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Sets vertical position for (row, col) sample points (1,0), (1,1), (1,2), (1,3), (1,4) (pixels) |
Bytes 2-3 |
Sets horizontal position for (row, col) sample points (0,1), (1,1), (2,1) (pixels) |
Bytes 4-5 |
Sets horizontal position for (row, col) sample points (0,3), (1,3), (2,3) (pixels) |
Sets positions of control points for Multipoint sPCC. |
Get Spcc Control Points | |
---|---|
Data returned is in the same format as the Write Parameter(s). | |
Returns positions of control points for Multipoint sPCC |
Set Pcc Coefficients Direct | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Point 0 = Row0 Col0 1 = Row0 Col1 2 = Row0 Col2 3 = Row0 Col3 4 = Row0 Col4 5 = Row1 Col0 6 = Row1 Col1 7 = Row1 Col2 8 = Row1 Col3 9 = Row1 Col4 10 = Row2 Col0 11 = Row2 Col1 12 = Row2 Col2 13 = Row2 Col3 14 = Row2 Col4 |
Bytes 1-2 |
Pcc Red R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 3-4 |
Pcc Red G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 5-6 |
Pcc Red B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 7-8 |
Pcc Green R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 9-10 |
Pcc Green G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 11-12 |
Pcc Green B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 13-14 |
Pcc Blue R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 15-16 |
Pcc Blue G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 17-18 |
Pcc Blue B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 19-20 |
Pcc Cyan R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 21-22 |
Pcc Cyan G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 23-24 |
Pcc Cyan B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 25-26 |
Pcc Magenta R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 27-28 |
Pcc Magenta G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 29-30 |
Pcc Magenta B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 31-32 |
Pcc Yellow R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 33-34 |
Pcc Yellow G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 35-36 |
Pcc Yellow B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 37-38 |
Pcc White R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 39-40 |
Pcc White G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 41-42 |
Pcc White B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
This command applies raw PCC Coefficients for all colors through direct access, for a specified sample point. Point is a number 0-15 corresponding to one of the the 5 x 3 PCC sample points in raster scan order. Note : This call will override any CCA settings performed by prior calls. |
Get Pcc Coefficients Direct | |
---|---|
Read Parameter(s) | |
Byte | Description |
Byte 0 |
Point 0 = Row0 Col0 1 = Row0 Col1 2 = Row0 Col2 3 = Row0 Col3 4 = Row0 Col4 5 = Row1 Col0 6 = Row1 Col1 7 = Row1 Col2 8 = Row1 Col3 9 = Row1 Col4 10 = Row2 Col0 11 = Row2 Col1 12 = Row2 Col2 13 = Row2 Col3 14 = Row2 Col4 |
Return Parameter(s) | |
Byte | Description |
Bytes 0-1 |
Pcc Red R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 2-3 |
Pcc Red G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 4-5 |
Pcc Red B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 6-7 |
Pcc Green R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 8-9 |
Pcc Green G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 10-11 |
Pcc Green B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 12-13 |
Pcc Blue R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 14-15 |
Pcc Blue G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 16-17 |
Pcc Blue B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 18-19 |
Pcc Cyan R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 20-21 |
Pcc Cyan G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 22-23 |
Pcc Cyan B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 24-25 |
Pcc Magenta R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 26-27 |
Pcc Magenta G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 28-29 |
Pcc Magenta B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 30-31 |
Pcc Yellow R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 32-33 |
Pcc Yellow G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 34-35 |
Pcc Yellow B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 36-37 |
Pcc White R Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 38-39 |
Pcc White G Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
Bytes 40-41 |
Pcc White B Range = 0.0 to 1.99951171875 with step size 0.00006103515 Format = s2.14 |
This command gets raw PCC Coefficients for all colors through direct access, for a specified sample point. Point is a number 0-15 corresponding to one of the the 5 x 3 PCC sample points in raster scan order. Note : This call will override any CCA settings performed by prior calls. |