JAJU788A June   2016  – May 2019 TPS3828

 

  1.   改訂履歴

Flashing Hybrid Wireless M-Bus/PLC Binary to CC1310 Using CCS™

This section explains how to flash the HYBRID-WMBUS-PLC software example binary on the CC1310 device using CCS. The instructions are in the following list:

  1. Connect the USB cable to the LAUNCHXL-CC1310 EVM.
  2. Launch the target configuration for CC1310 and connect to the device in the CCS debug mode
  3. Select Run → Load → Load Program and flash HybridWmbusPlcExample_CC1310_LAUNCHXL_tirtos_ccs.out under the debug directory.