JAJU802A January 2022 – October 2022
When MOSFET is in OFF state, it will have to block DC bus voltage which can rise up to 400V maximum. S0, with leaving 50% room as safety factor, 600V MOSFET is selected in this design.
When MOSFET is ON, it will conduct peak value of inductor current when inductance is at its lowest value
Total power dissipation in MOSFET consists of conduction loss, turn off loss, turn on loss, COSS loss and gate drive loss. It can be estimated using following formula
Conduction loss in MOSFET can be calculated by following formula
where FET RMS current can be calculated using following formula:
Where COSS varies with line voltage and is not a linear function. The following equation and information from the FETs data sheet can be used to calculate COSS(AVG). COSS(SPEC)is the typical COSS measured at a specified voltage VDS(SPEC).