SBAA535A March 2022 – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024
Some ADCs include a programmable delay time to accommodate external settling requirements. Table 5-3 shows the ADS124S08 available programmable delay time options in terms of one modulator period, tMOD.
| BIT | FIELD | TYPE | RESET | DESCRIPTION |
|---|---|---|---|---|
| 7:5 | DELAY[2:0] | R/W | 0h | Programmable conversion delay selection Sets the programmable conversion delay time for the first conversion after a WREG when a configuration change resets the digital filter and triggers a new conversion. 000 : 14 ∙ tMOD (default) 001 : 25 ∙ tMOD 010 : 64 ∙ tMOD 011 : 256 ∙ tMOD 100 : 1024 ∙ tMOD 101 : 2048 ∙ tMOD 110 : 4096 ∙ tMOD 111 : 1 ∙ tMOD |
The delay shown in Table 5-3 can be used for several reasons, including waiting for an external analog RC filter to settle to a final value, accommodating the PGA start-up time, or ensuring that an integrated voltage reference or current source (IDAC) is stable before starting the conversion process.
Programmable delay time was included in Figure 4-7 and Figure 5-2, though not explicitly mentioned. Figure 5-3 shows a complete diagram for the ADS124S08 low-latency and sinc3 filter behavior in single-shot conversion mode. The programmable delay time corresponds to the yellow boxes, as per the legend in the top right.
As Figure 5-3 shows, the programmable delay occurs immediately after a conversion start is triggered. Therefore, this time period only needs to be considered when calculating first conversion latency. However, the programmable delay time is not always included in the overall conversion latency table values. Table note #3 for the ADS124S08 conversion latency table specifically states that the conversion latency values do not include the default programmable delay time of 14 ∙ tMOD seconds. Comparatively, the table note for the ADS1261 conversion latency table states that the conversion latency values do include the default 50-µs programmable delay time. Refer to the specific ADC data sheet to determine if that device has a programmable delay feature as well as how that time affects the overall conversion latency.