SBAA535A March 2022 – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024
Table 8-8 reports ∙ the system parameters that determine the cycle time in Example #4:
| PARAMETER | VALUE |
|---|---|
| ADC | ADS124S08 |
| ODR | 1000 SPS |
| Filter type | Low-latency |
| Clock frequency | 3 MHz |
| Conversion mode | Single-shot |
| Programmable delay | 14 ∙ tMOD (default) |
| Chopping | Disabled |
| Conversions per channel | 3 |
| # of channels | 2 |
Example #4 keeps all of the same system parameters as Example #3, though the default clock frequency, fCLK, of 4.096 MHz has been changed to a new clock frequency, fCLK_NEW, of 3 MHz. This choice directly affects the conversion latency and the programmable delay, and indirectly affects the ODR.
While not shown in this document, the ADS124S08 data sheet identifies the first-conversion latency, tFC, using the low-latency filter at ODR = 1000 SPS as 296 ∙ tMOD periods. Using the conversion latency in terms of tMOD periods instead of milliseconds enables easier calculations because the number of tMOD periods is independent of clock frequency.
The conversion latency of 296 ∙ tMOD periods includes the ADC overhead but does not include the programmable delay, tDELAY. Using the default value of tDELAY = 14 ∙ tMOD, the total first-conversion latency, tFC_TOTAL, is given by Equation 18:
Next, Equation 19 calculates one tMOD period in terms fCLK_NEW using the ADS124S08:
At fCLK_NEW = 3 MHz, tMOD = 5.33 µs. Therefore, tFC_TOTAL = 310 ∙ 5.33 µs = 1.652 ms
Finally, there is no need to consider additional latency due to chopping. Equation 21 calculates the cycle time, tCYCLE, using the scan time for one channel, tCH, that results from Equation 20. This assumes that the user starts the next conversion on each channel immediately after the previous conversion result is ready:
Ultimately, the cycle time for this example is 9.912 ms for 6 conversion results. Figure 8-4 depicts a timing diagram for the example system given the design parameters.