SBAU378A September 2021 – January 2022 ADS1148 , ADS1248
The ADS1x48EVM board includes provisions for using a PCB-mounted thermistor to measure the cold junction of a thermocouple connected to the TC+ and TC– inputs on J5. As Figure 3-11 shows, top- and bottom-layer copper pours create an isothermal bridge between the NTC± and TC± inputs. This bridge helps ensure that thermistor RT1 measures the same temperature as the thermocouple cold junction at inputs J5:1 and J5:2, enabling a more accurate thermocouple measurement.
Figure 3-11 PCB Layout for J5 Terminal
Block Showing Copper Pours for CJC MeasurementAs discussed in Section 3.5.2 and in Figure 3-9, thermistor RT1 is not populated by default on the ADS1x48EVM. Choose a 10-kΩ NTC thermistor in a 0603 package for this component. To measure the thermistor voltage, follow the steps outlined at the end of Section 3.5.2, noting that step #1 (connect the sensor) is satisfied by soldering the thermistor (RT1) to the PCB. Also, the ADS1x48 is a multiplexed ADC and therefore can only measure one single-ended or differential input per conversion cycle. As a result, the thermocouple and CJC measurements must be taken separately and then manipulated in software to determine the resulting temperature. To learn more about CJC as well as how to use this value to determine the true measured temperature, see the A Basic Guide to Thermocouple Measurements application report.