SBAU390 September 2021 TMAG5170 , TMAG5170 , TMAG5170-Q1 , TMAG5170-Q1 , TMAG5173-Q1 , TMAG5173-Q1 , TMAG5273 , TMAG5273
This slider attachement uses an N42 grade cylindrical magnet as a magnetic field source to demonstrate the ability of TMAG5170 to track linear motion of a nearby magnet. The magnet is glued into the slider object, which then may pass freely down the length of the slider track. Tracking Slide-By Displacement with Linear Hall-Effect Sensors (SBAA513).
Nylon components were selected as they are non-magnetic and will not interfere with the magnetic field and bond well when glued.