SBOA550 October   2022 OPA1671 , OPA2990 , SN74HCS04 , SN74HCS164 , SN74HCS30 , SN74LVC1G00 , SN74LVC1G123 , TLC04 , TLC14 , TS5A9411

 

  1.   Abstract
  2.   Trademarks
  3. Introduction
  4. The Davies Generator
  5. Optimizing Standard Resistance Values for THD Performance
  6. Simulation Examples
  7. Compensating for Shift Register Output Resistance
  8. Voltage-Mode Thevenin Equivalent
  9. Harmonic Filtering
  10. Tracking Harmonic Filter
  11. Multiphase Output
  12. 10Conclusion
  13. 11Acknowledgment
  14. 12References
  15.   A Analytical Solution for Resistance Network Values
  16.   B Forbidden States of the Johnson Counter

Multiphase Output

Additional coherent phases may be derived from the same shift register. By driving additional resistor networks with delayed outputs 2, 3, 4 or more phased outputs can be created. The 6-bit Johnson counter is the shortest length that can create 2, 3, or 4 phase outputs, even simultaneously when driven as shown throughout Figure 8-1.

Figure 9-1 6-bit Johnson Counter can Generate Various Useful Phase Relationships; 90°, 120°, 180°, 240°, 270°

The simulation results of Figure 8-1 are found in Figure 8-2. For simplicity, output filtering has been omitted from these results. Note that variation in harmonic filter components can cause unwanted phase shift between outputs.

Figure 9-2 Multiphase Output Simulation