SBOU128B february 2013 – july 2023 INA231
The INA231 device has a flexible I2C address configuration that allows multiple devices on the same I2C lines. By moving the A0 and A1 addresses on jumpers J3-J6 to either GND, VS, SDA or SCL, the user can change the INA231to a total of 16 I2C addresses (see Table 5-1).
| A1 | A0 | TARGET ADDRESS |
|---|---|---|
| GND | GND | 1000000 |
| GND | VS+ | 1000001 |
| GND | SDA | 1000010 |
| GND | SCL | 1000011 |
| VS+ | GND | 1000100 |
| VS+ | VS+ | 1000101 |
| VS+ | SDA | 1000110 |
| VS+ | SCL | 1000111 |
| SDA | GND | 1001000 |
| SDA | VS+ | 1001001 |
| SDA | SDA | 1001010 |
| SDA | SCL | 1001011 |
| SCL | GND | 1001100 |
| SCL | VS+ | 1001101 |
| SCL | SDA | 1001110 |
| SCL | SCL | 1001111 |
Figure 5-3 shows how to configure the I2C addresses. Click the A0 or A1 box and select how to configure the hardware on the EVM. Failure to select the correct address prevents the INA231 device from communicating with the software.
Figure 5-3 Setting the A1
Address