SLAAE72 December 2022 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
I/O setting is the most common problem causing unexpected high-power consumption.
For unused pins, the IOMUX configuration should remain in the default (high-Z) state.
For the digital input pin used, please pay attention to the internal pull-up or pull-down resistor. If the input voltage is incompatible, leakage current will be caused. When the input voltage is VCC or VSS, the digital input pin consumes the least power. If the voltage is between VCC or VSS, the internal MOSFET will be biased in the linear region and will consume a lot of power. This usually occurs when unused digital input pins float.
For the digital output pin used, when entering low-power mode, please pay attention that the last valid IO output state may be latched, if no further inversion control. It may cause the additional power consumption.