SLAAEN0 September 2024 MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Tamper I/O is a general purpose input/output (GPIO) sourced using the VBAT domain and with two modes of operation in LFSS. The output of the I/O pin is able to drive a low-current LED from the VBAT domain. The tamper input and output are used to detect tamper events such as a voltage transition on the input pin or an output that can enable or disable peripherals. Tamper I/O is often used in Alarm control systems, Microsoft® Windows® security, and so forth.