Custom_Element is the structure
defined in user_define.h. Custom_Element is also shown in Figure 2-5.
Origin Identifier indicates the origin
of the message. The following are the examples(CAN_ID_LENGTH =0,UART_ID_LENGTH
=4).
- Example 1 - CAN interface
receive and transmit
- When CAN-UART bridge receives a CAN message, the ID from the CAN
frame is the Origin Identifier, which indicates where the
message came from.
- When CAN-UART bridge transmits a CAN message, Origin Identifier will
be ignored(CAN_ID_LENGTH is set to 0 default).
- Example 2 - UART interface
receive and transmit (UART protocol transmission)
- When CAN-UART bridge receives the UART message(UART protocol
transmission), DEFAULT_UART_ORIGIN_ID is the Origin
Identifier since the UART does not have an ID.
- When CAN-UART bridge transmits the UART message(UART protocol
transmission), Origin Identifier will be 4-byte ID in UART
data(UART_ID_LENGTH is set to 4 default), indicating where the
message came from.
- Example 3 - UART interface
receive and transmit (UART transparent transmission)
- When the CAN-UART bridge receives the UART message (UART transparent
transmission), DEFAULT_UART_ORIGIN_ID is the Origin
Identifier since the UART does not have an ID.
- When the CAN-UART bridge transmits the UART message (UART
transparent transmission), Origin Identifier will be ignored
(Transparent transmission does not have an ID area).
Destination Identifier
indicates the destination of the message. The following are the
examples(CAN_ID_LENGTH =0,UART_ID_LENGTH =4).
- Example 1 - CAN interface receive
and transmit
- When the CAN-UART bridge receives a CAN message, the
DEFAULT_CAN_DESTINATION_ID is the Destination Identifier since
the CAN_ID_LENGTH is set to 0 by default. UART transmit does not require
an ID.
- When the CAN-UART bridge transmits a CAN message, Destination
Identifier will be CAN ID in CAN frame. In this example, 11 bit
or 29 bit are both supported.
- Example 2 - UART interface
receive and transmit (UART protocol transmission)
- When the CAN-UART bridge receives a UART message (UART protocol
transmission), the 4-byte ID from UART data is the Destination
Identifier (UART_ID_LENGTH is set to 4 default). The CAN
transmit requires ID information.
- When the CAN-UART bridge transmits a UART message (UART protocol
transmission), Destination Identifier will be ignored since UART
transmit does not require an ID.
- Example 3 - UART interface
receive and transmit (UART transparent transmission)
- When CAN-UART bridge receives UART message (UART transparent
transmission), DEFAULT_UART_DESTINATION_ID is the Destination
Identifier. (Transparent transmission does not have an ID area).
CAN transmit requires ID information.
- When the CAN-UART bridge transmits a UART message (UART transparent
transmission), Destination Identifier will be ignored since UART
transmit does not require an ID.
/*user-defined information storage structure */
typedef struct {
/*! Origin Identifier, indicating the origin of the message */
uint32_t origin_id;
/*! Destination Identifier, indicating the destination of the message */
uint32_t destination_id;
/*! Data Length Code */
uint8_t dlc;
/*! Data bytes */
uint8_t data[TRANSMIT_DATA_LENGTH];
} Custom_Element;