SLAU318G July   2010  – March 2016

 

  1.   MSP-EXP430G2 LaunchPad™ Development Kit
    1.     Trademarks
    2. 1 Preface: Read This First
      1. 1.1 If You Need Assistance
      2. 1.2 Related Documentation From TI
    3. 2 MSP-EXP430G2 LaunchPad™ Development Kit Overview
      1. 2.1 Overview
      2. 2.2 Features
      3. 2.3 Kit Contents
      4. 2.4 Revisions
    4. 3 Installation
      1. 3.1 Download the Required Software
      2. 3.2 Install the Software
      3. 3.3 Install the Hardware
    5. 4 Getting Started With MSP-EXP430G2 LaunchPad™ Development Kit
      1. 4.1 Getting Started
      2. 4.2 Demo Application, Internal Temperature Measurement
    6. 5 Develop an Application With the MSP-EXP430G2 LaunchPad™ Development Kit
      1. 5.1 Developing an Application
      2. 5.2 Program and Debug the Temperature Measurement Demo Application
      3. 5.3 Disconnect Emulator From Target With Jumper J3
      4. 5.4 Program Connected eZ430™ Target Boards
      5. 5.5 Connecting a Crystal Oscillator
      6. 5.6 Connecting a BoosterPack™ Plug-in Module
      7. 5.7 Supported Devices
      8. 5.8 MSP-EXP430G2 On-Board Emulator
    7. 6 MSP-EXP430G2 Hardware
      1. 6.1 Device Pinout
      2. 6.2 Schematics
      3. 6.3 PCB Layout
      4. 6.4 Bill of Materials (BOM)
    8. 7 Suggested Reading
    9. 8 Frequently Asked Questions (FAQ)
  2.   Revision History

Suggested Reading

The primary sources of information on MSP430 MCUs are the device-specific data sheets and the family user's guides. The most up-to-date versions of those documents can be found at the TI MSP430 landing page.

For more information on CCS and IAR, download the latest version from http://www.ti.com/mspds and read the included user's guides and documentation in the installation folder. Documents describing the IAR tools (Workbench/C-SPY, the assembler, the C compiler, the linker, and the library) are located in common\doc and 430\doc. All necessary CCS documents can be found in the msp430\doc folder in the CCS installation path. The FET user's guide also includes detailed information on how to set up a project for the MSP430 MCUs using IAR or CCS, and it is included in most of the IDE releases and on the TI MSP430 MCU website.