SLAU646F September 2015 – June 2020
The
README-build.sh
bash script included with the source-full package (and in the source-patches package) can be used to build the toolchain for Windows, Linux and macOS hosts. The script contains some distribution-specific instructions on how to install the pre-requisite tools from Section 6.1.
To build native Linux and macOS toolchains, follow the instructions in Section 6.2.1.
To build the toolchain for Windows hosts, follow both the instructions in Section 6.2.1 and then Section 6.2.2.
If less than 2 GB of RAM is available during the build, the build may fail.