SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The flash controller manages all program, erase, and verification operations performed on the nonvolatile memory system. It contains memory-mapped registers in the peripheral region of the device memory map which must be configured by software to perform operations on the flash memory.
TI provides software abstraction for the flash controller as a part of the DriverLib layer of the software development kit (SDK). It is recommended to use the DriverLib abstraction layer when operating on the flash memory with software, but it is not mandatory to do so. To use the DriverLib software abstraction layer to perform operations on the flash memory, review the software development kit (SDK) documentation provided separately from this document. To directly operate on the flash memory with using low level register accesses to the flash controller, review the remainder of this section in detail.