SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Most peripherals on the device contain an input clock selection mux which is used to select, and optionally divide down, the functional clock for the peripheral. Figure 2-8 shows the superset peripheral clock selection mux and optional clock divider. Note that not every peripheral has every clock source shown in Figure 2-8. For example, accelerators such as CRC, and DMA run off of the bus clock. There is no option to select MFCLK or LFCLK for these peripherals. To determine the available clock sources for a peripheral, see the chapter for the specific peripheral and review the clock input selections.
Exceptions
There are also several peripherals that have a unique clock selection scheme and do not use the standard peripheral clock mux shown above. Typically this is due to a requirement for a peripheral to have a clock source that is asynchronous to the rest of the system. Cases where this occurs include: