SLAU847E October 2022 – May 2025 MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
SWD security level 0 is the least restrictive SWD security state. This is the default state of a new device from TI, and it is also the state of a device following a successful factory reset. There are no restrictions on application debug access, mass erase, factory reset, for failure analysis in this state.
When to Use This State
Level 0 is well suited for prototyping and development, as it allows programming of the device memory and debug of the processor and peripherals.
When to Not Use this State
Level 0 should not be used in mass production. An attacker would have full freedom to read the contents of the device memory, manipulate the execution of the device, and possibly change the flash memory contents (depending on the flash memory write protection scheme).