SLOA292 May   2020 TAS5760LD

 

  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
      1.      6
    5.     7
      1.      8
      2.      9
    6.     10
      1.      11
      2.      12
      3.      13
      4.      14
    7.     15
    8.     16

Conventional Solution With External BJT Switch

If the design still cannot resolve the pop noise, the conventional solution is that the SOC uses general-purpose input/output (GPIO) to control the external BJT. Figure 15 shows the implementation on how to use BJT at the output stage.

sloa292-system-processor-control-external-bjt-before-system-turns-off.gifFigure 15. System Processor Control External BJT Before System Turns Off