SLUAAH0 February   2022 UCC14130-Q1 , UCC14131-Q1 , UCC14140-Q1 , UCC14141-Q1 , UCC14240-Q1 , UCC14241-Q1 , UCC14340-Q1 , UCC14341-Q1 , UCC15240-Q1 , UCC15241-Q1

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Pin Configuration and Functions
  3. Three-Phase Traction Inverter
  4. Gate Drive Bias Requirements
    1. 3.1 Gate Drive Bias Architectures
    2. 3.2 IGBT vs. SiC
    3. 3.3 Determining Required Bias Supply Power
    4. 3.4 Input Voltage Requirements
    5. 3.5 Output Voltage Requirements
  5. Single Positive Isolated Output Voltage
  6. Dual Positive and Negative Output Voltages
  7. Dual Positive Output Voltages
  8. Capacitor Selection
  9. RLIM Current Limit Resistor
    1. 8.1 RLIM Functional Description
    2. 8.2 RLIM Dual Output Configuration
      1. 8.2.1 CVEE Above Nominal Value CVDD Below Nominal Value
      2. 8.2.2 CVEE Below Nominal Value CVDD Above Nominal Value
      3. 8.2.3 Gate Driver Quiescent Current: IQ_VEE > IQ_VDD
      4. 8.2.4 Gate Driver Quiescent Current: IQ_VEE < IQ_VDD
      5. 8.2.5 CVEE Above Nominal Value CVDD Below Nominal Value: IQ_VEE > IQ_VDD
      6. 8.2.6 CVEE Below Nominal Value CVDD Above Nominal Value: IQ_VEE < IQ_VDD
    3. 8.3 RLIM Single Output Configuration
  10. UCC14240-Q1 Excel Design Calculator Tool
  11. 10Thermal Considerations
    1. 10.1 Thermal Resistance
    2. 10.2 Junction-to-Top Thermal Characterization Parameter
    3. 10.3 Thermal Measurement and TJ Calculation Example
  12. 11Enable (ENA) and Power Good (/PG)
  13. 12PCB Layout Considerations
  14. 13Reference Design Example
  15. 14Summary
  16. 15References

Enable (ENA) and Power Good (/PG)

The UCC14240-Q1 includes a primary referenced, 5-V TTL and 3.3-V LVTTL logic compatible, active-high enable function. Forcing ENA low disables the device, and places it in a non-switching standby mode where current consumption is reduced to less than 500 µA. Pulling the ENA pin high, above the 2-V threshold, activates normal device functionality. The ENA pin has a weak internal pull-down resistor, so the ENA pin floats to the disable state if the pin is left open. If ENA is not used it should be pulled high a voltage between 2.5 V<VENA<5.5 V. Care should be taken to assure VENA does not exceed 5.5 VMAX.

The active-low, power good (/PG) pin is an open-drain output that indicates when the UCC14240-Q1 has no faults present and the output voltages are within ±10% of their regulation setpoints. Connect a pull-up resistor (>1 kΩ) from the /PG pin to either a 5-V or 3.3-V logic rail. For applications not using the /PG signal, /PG can be connected directly to GNDP.

The start-up waveforms in Figure 11-1 show the expected behavior of /PG relative to ENA. The input voltage (VIN=24 V, not shown) is already present and the UCC14240-Q1 is activated by ENA going high. The measured time between ENA high and /PG low is ~3.75 ms but can vary according to the time required for the isolated output voltages to be within ±10% of the set regulation value. The longer time required for COM-VEE to reach regulation relative to VDD-VEE results in the slight VDD-COM overshoot but this is happening before /PG reaches its active-low state. This emphasizes the importance of not switching the gate driver until /PG is in the active-low state. Note that the waveforms introduced here, were captured from the UCC14240EVM-052 EVM. Using the UCC14240EVM-052 for Biasing Traction Inverter Gate Driver ICs Requiring Single, Positive or Dual, Positive/Negative Bias Power is the EVM User's Guide containing the schematic, PCB details and measured performance data.


GUID-20220126-SS0I-NLZT-Q3D2-RNZKDCPP6W9W-low.png

Figure 11-1 Start-up: VIN=24 V, IDD=80 mA, (top: VISO (VDD-VEE), 10V/div, mid-1: COM, 2V/div, mid-2: VDD=VISO-COM, 10V/div, mid-3: VEE=-COM, 5V/div, mid-4: /PG, 5V/div, bot: ENA, 5V/div), time = 2ms/div unless otherwise noted.

Conversely, the shut-down waveforms in Figure 11-2 show that as soon as ENA is pulled low, the UCC14240-Q1 output voltage are discharged in a controlled manner and /PG transitions high with almost no delay relative to ENA.


GUID-20220126-SS0I-HKRJ-2G0D-SNF0TZXFQLVK-low.png

Figure 11-2 Shutdown: VIN=24 V, IVDD=80 mA, (top: VISO (VDD-VEE), 10V/div, mid-1: COM, 2V/div, mid-2: VDD=VISO-COM, 10V/div, mid-3: VEE=-COM, 5V/div, mid-4: /PG, 5V/div, bot: ENA, 5V/div), time = 2ms/div unless otherwise noted.