SLUUA65E april 2014 – june 2023 BQ28Z610
Floating point values are stored using the IEEE754 Single Precision 4-byte format in Little Endian byte order.
| 0 | 1 | 2 | 3 |
| Fract [0–7] | Fract [8–15] | Exp[0] + Fract[16–22] | Sign + Exp[1–7] |
Where:
Exp: 8-bit exponent stored with an offset bias of 127. The values 00 and FF have special meaning.
Fract: 23-bit fraction. If the exponent is > 0, then the mantissa is 1.fract. If the exponent is zero, then the mantissa is 0.fract.
The floating point value depends on the special cases of the exponent: