SLUUBT4B June 2018 – June 2025 BQ40Z80
The Board Offset calibration option is not offered in Battery Management Studio, because this is not required when using the bq40z80EVM. The Board Offset calibration option is available in bqProduction.
Current can also be calibrated using the FETs. Measure the current in the discharge path and enter this value in the Applied Current field.