SLUUCU7 November 2023 BQ25960H
Table 3-1 lists the BQ25960HEVM board connections and ports.
| Jack | Description | |
|---|---|---|
| J1 | VIN1 | Positive rail of the priority input adapter or power supply |
| GND | Ground | |
| J2 | VOUT | Positive rail of the charger battery input |
| BATP | Input connected to the positive terminal of the battery for remote battery voltage sensing | |
| BATN | Input connected to the negative terminal of the battery for remote battery voltage sensing | |
| PACK- | Negative rail of the charger battery input | |
| J3 | VIN2 | Positive rail of the secondary input adapter or power supply |
| GND | Ground | |
| J4 | VBUS | Positive rail of the VBUS input to the charger ICs |
| GND | Ground | |
| J5 | Communication port | I2C communication port for use with the USB2ANY interface adapter |
| J6 | Communication port | I2C communication port for use with the EV2400 interface board |
| J7 | VSYS | Positive rail of the BQ25611D charger's system output voltage |
| GND | Ground | |
| J8 | USB-C connector | Provides power to VIN2 and has D+/D- lines for input source detection |
Table 3-2 below lists the jumper connections available on this EVM.
| Jumper | Description | Single BQ25960H Setting | Dual BQ25960H Setting |
|---|---|---|---|
| JP1 | BATP to VOUT connection. | Installed | Installed |
| JP2 | ACDRV1 to GND connection. Connect this jumper if powering directly from VBUS, or if ACFET1/RBFET1 are removed. | Not installed | Not installed |
| JP3 | U1 TSBAT or SYNCOUT connection. Connect to SYNCOUT if operating in primary/secondary mode. | Installed between left pin and middle pin (connect to TSBAT) | Installed between middle pin and right pin (connect to SYNCOUT) |
| JP4 | ACDRV2 to GND connection. Connect this jumper if ACFET2/RBFET2 are removed. | Not installed | Not installed |
| JP5 | U1 /INT pin connection to 1.2V pull-up rail. | Installed | Installed |
| JP6 | U1 REGN pin connection to U1 TSBUS resistor network. | Installed | Installed |
| JP7 | Different resistor connection for U1 TSBUS resistor network. | Installed | Installed |
| JP8 | U2 I2C address and mode selection. | Installed | Installed |
| JP9 | U1 I2C address and mode selection. | Not installed | Installed between top pin and middle pin (connect to R16) |
| JP10 | U1 TSBUS pin connection to U1 TSBUS resistor network. | Installed | Installed |
| JP11 | U2 TSBAT connection to TSBAT resistor network. | Installed | Installed |
| JP12 | U2 REGN pin connection to U2 TSBUS resistor network. | Installed | Installed |
| JP13 | SDA and SCL connection to 1.2V I2C pull-up rail. | Installed | Installed |
| JP14 | Different resistor connection for U2 TSBUS resistor network. | Installed | Installed |
| JP15 | U2 /INT pin connection to 1.2V pull-up rail. | Installed | Installed |
| JP16 | U2 TSBUS pin connection to U2 TSBUS resistor network. | Installed | Installed |
| JP17 | Connection from TSBAT resistor network to either U1 REGN pin or U2 REGN pin. | Installed between top pin and middle pin (connect to REGN_M) | Installed between top pin and middle pin (connect to REGN_M) |
| JP18 | Input selection for 1.2V LDO | Installed between top pin and middle pin (connect to VOUT) | Installed between top pin and middle pin (connect to VOUT) |
| JP19 | Different resistor connection for TSBAT resistor network. | Installed | Installed |
| JP20 | D- connection for USB-C connector. | Installed | Installed |
| JP21 | Charge enable connection for U4. | Installed | Installed |
| JP22 | D+ connection for USB-C connector. | Installed | Installed |
| JP23 | U4 thermistor NORMAL temperature setting. Install this jumper to simulate entering normal temperature region. | Installed | Installed |
Out of the box, the BQ25960HEVM is configured to evaluate the performance of the BQ25960H only. If the BQ25611D must also be evaluated, then the user needs to populate R29 and R32, as shown in the schematic in Figure 6-3.