Follow the connection procedure below and Figure 3-1 can be used as a reference.
- Make sure all the output of the function generator, and voltage source are off before connection.
- Function generator Ch-A channel applied on IN_IN.
- Power Supply:
- Power supply #1: positive node connected
to input of DMM #1 and DMM #1 output connected to test point marked as
VCC, negative node of Power Supply #1 connected directly to test point
marked as GND.
- Power supply #2:
negative node connected to OCP_IN and positive node connected to
GND or GND_IO (whichever is more convenient), this makes it so OCP_IN
sees -5V, not 5V.
- Oscilloscope:
- VDD Signal:
Connect oscilloscope Ch-1 probes to test points marked as VDD to
GND, smaller measurement loop is preferred.
- IN Signal: Connect
oscilloscope Ch-2 probes to test points marked as IN to GND,
smaller measurement loop is preferred.
- OUT Signal:
Connect oscilloscope Ch-3 probes to test points marked as GATE to
GND, smaller measurement loop is preferred.
- FLTb Signal:
Connect oscilloscope Ch-4 probes to test points marked as EN/FLT to
GND, smaller measurement loop is preferred.