SLVUBZ4 February   2021 TPS25750

 

  1.   Trademarks
  2. 1Getting Started
    1. 1.1 Related Documents
    2. 1.2 Hardware
    3. 1.3 Software
    4. 1.4 Installation and Launch
      1. 1.4.1 Web Browser
      2. 1.4.2 Native Application
    5. 1.5 TPS25750 Application Customization Tool Features
  3. 2Using the TPS25750 Application Customization Tool
    1. 2.1 Default View
    2. 2.2 Filling Out The Form
    3. 2.3 Generating a New Configuration
    4. 2.4 Exporting and Importing Settings
    5. 2.5 Generating The Binary
    6. 2.6 Flashing To The Hardware
  4. 3Example Configuration

Example Configuration

This section will walk through setting up a new configuration, filling out the form, and flashing to the device. A TPS25750EVM is needed to execute the final step. If one is not available, the remainder of the example can still be followed.

  • Select the New Configuration button on the right side panel. See Figure 3-1.
GUID-20200807-CA0I-29BC-L4BB-RW4LBHZBZCL2-low.png Figure 3-1 Button to generate a new configuration is pointed to by the arrow
  • When the modal appears, click the red New configuration button, as shown in Figure 3-2. This will reset any existing configuration on the form.
GUID-20200807-CA0I-G4S0-NVQC-MTMQ4VZQTV8X-low.png Figure 3-2 New configuration can be generated by clicking the button pointed to by the arrow
  • Question one should already be filled out. Ensure that the top-left option is selected.
GUID-20200807-CA0I-B0FG-K7ZP-0GJRNZCCT4CN-low.png Figure 3-3 Ensure that the option outlined in black is selected
  • Question two should also be answered already. Ensure that 100W (20V) is selected. See Figure 3-3.
  • Question three should already be filled out as well. Ensure that 100W (20V) is selected. See Figure 3-3.
  • Question four should also be filled out. Ensure that Host & Device - Dual Role Port (DRP) is selected. See Figure 3-3.
  • Select Power source (provider) as the answer to question five. See Figure 3-3.
GUID-20200807-CA0I-FTJM-KSHW-CCBHTFSJ3CKX-low.png Figure 3-4 Ensure that the options pointed to by the arrows are selected
  • Select the USB 3.2 Gen 2 option for question six.
  • For question seven, select No, use the TI Vendor ID in the Vendor Information File (VIF).
  • For question eight, select No, use '0x0000' as the Product ID.
GUID-20200807-CA0I-VT51-RNS8-LTQXPGHC90N2-low.png Figure 3-5 Ensure that the options pointed to by the arrows are selected
  • Select BQ25790 or BQ25792 as the battery charger to integrate for question nine.
  • Enter 3.7V as the battery charging voltage for the question ten.
  • Enter 1A as the battery charging current for the question eleven.
GUID-20200807-CA0I-RCDH-99CM-9TXHTS5Z1WLB-low.png Figure 3-6 Ensure that the answers to the battery charger questions match those shown by the arrows
  • The Flash Device button on the right side panel should now be enabled. Ensure that the TPS25750EVM is physically connected to the computer through USB, and click the Flash Device button to upload the new settings onto the device.
GUID-20200807-CA0I-TNG0-KP8C-M9B7CQ6ZSKZ7-low.pngFigure 3-7 After filling out the form, click the button to flash to the device, pointed to by the arrow