SLVUC05A November 2020 – July 2022 TPS25750
Description | The 'GSrC' Task instructs PD Controller to issue a Get_Source_Capmessage to the Port Partner device at the first opportunity while maintainingpolicy engine compliance. |
---|---|
INPUT DATAX | None. |
OUTPUT DATAX | Byte 1: Standard Task Return Code. See also Table 3-1. |
Task Completion | The 'GSrC' Task completes either when the Source Capabilities message is received or the Task otherwise fails. The 'GSrC' Task shall be considered rejected if:
|
Side Effects | When the 'GSrC' Task completes successfully the RX_SOURCE_CAPS register (0x30) will have been updated. |
Additional Information | None. |