The TPS25990EVM provides an add-on circuit
to facilitate load transients and persistent overcurrent events. The implementation consists
of three low side MOSFETs (Q4, Q5, and Q6) and a mono-shot gate driver circuit (U7 and U8)
as well as six onboard load resistors of 1 Ω each (R45 to R50) in parallel. Using a single
pole single through (SPST) switch (S1), the mono-shot gate driver generates a gate signal
lasting 1 ms, 2 ms, 5 ms, 10 ms, and 20 ms. By pressing the switch SW3, the low side MOSFETs
are turned on for that specific duration, creating a load transient on the steady-state load
above. Use the following instructions to apply a load transient or persistent overcurrent
event using this onboard switching circuit:
- The overcurrent blanking timer duration
(tTIMER) is 2.18 ms by default. The overcurrent blanking timer duration can
be programmed via PMBus using the OC_TIMER (E6h) register if another timer duration is
needed in the range of 0 ms to 27.8 ms.
- The reference voltage for overcurrent
protection and active current sharing is at 1 V by default. The reference voltage can also
be programmed via PMBus using the VIREF (E0h) register if another reference voltage is
needed in the range of 0.3 V to 1.2 V.
- Configure the jumper J6 in a good
position to set required circuit breaker threshold (IOCP) as per Table 4-3.
- Set the input supply voltage VIN to 12 V
and current limit to 200 A.
- Connect the power supply between VIN
(Connector T1) and PGND (Connector T3) and enable the power supply.
- Connect a steady-state load between VOUT
(Connector T2) and PGND (Connector T3).
- Use the single pole single through (SPST)
switch (S1) to configure the transient load turn on duration. Press the switch SW3 to turn
on the Q4, Q5, and Q6 MOSFETs, which creates a load transient of 72 A (typical) between
VOUT and PGND with 12 V output.
- Observe the waveforms of VOUT (TP4),
MOSFET GATE (J9), and input current using an oscilloscope.
Another option is to apply a custom load
transient using an external function generator, connected between TP30 and TP31, and the
shunt of jumper J9 set to "2-3".
CAUTION: In that case, make sure to
limit the transient load current magnitude to a safe level for reliable operation of the
load resistors (R45 to R50) based on their maximum permissible peak pulse power vs pulse
duration plot.
Figure 5-13 and Figure 5-14 show the test waveforms of transient overload and persistent overload events respectively
using the onboard switching circuit.
Figure 5-13 Transient Overload Performance in
TPS25990EVM Using the Onboard Switching Circuit (VIN = 12 V,
tITIMER = 14 ms, COUT = 1470 μF, RIMON = 1.47 ∥ 1.1
kΩ, VIREF = 1 V, IOUT(Steady-State) = 85 A, and
IOUT(Transient) = 65 A for 9 ms)
Figure 5-14 Persistent Overload Performance in
TPS25990EVM Using the Onboard Switching Circuit (VIN = 12 V,
tITIMER = 14 ms, COUT = 1470 μF, RIMON = 1.47 ∥ 1.1
kΩ, VIREF = 1 V, IOUT(Steady-State) = 85 A, and
IOUT(Transient) = 65 A for 18 ms)