SLYU058D May 2021 – February 2024 TMAG5173-Q1 , TMAG5273
If desired, the SCB can communicate directly with the EVM without the use of the GUI through the USB serial (COM) port. Simply send the desired command string over the serial port and receive the results. This is useful for interfacing the EVM with custom setups/scripts/GUIs. Note that the TMAG5x73EVM must be connected to the SCB to receive any command responses from the SCB.
To read and write registers, follow the below format:
Figure 4-18 Example Register Read
ResponseThe number to the right of value represents the value read from the register. Note that this value is represented in decimal form and not hexadecimal.
Figure 4-19 Example
Register Write ResponseOther useful commands include the following:
Figure 4-20 Example
Firmware Revision Command Response
Figure 4-21 Firmware
Revision Version in GUI About Screen
Figure 4-22 BSL Command
ResponseTrigger conversion command format: rreg 0