SNOU150D January 2018 – April 2025 LMG1020
The test points on this EVM have been designed for use with oscilloscope probes with the included spring-type ground connections, often called pigtails. Using the small pigtails without the probe clips will minimize measurement error and produce a cleaner signal with the fast switching GaN devices used on this EVM. The data shown in this user guide has been obtained using such a measurement method.
| TEST POINT | NAME | DESCRIPTION |
|---|---|---|
| TP1 | 5 V | Connected to the VDD pin of the LMG1020. This is 5Vdc nom |
| TP2 | VCC | Connected to the Vin of the on board LDO, this is the input bias supply voltage (5.5V-15Vdc) |
| TP3 | GND | Connected to GND, the common reference for the board |
| TP4 | Vg | Gate voltage, connected to the Gate of the GaN FET |
| TP5 | VBUS | Connected to the positive of the input supply for the power stage |
| TP6 | K | Connected to the cathode of the laser diode, or negative of the unpopulated load. This is also the drain of the GaN FET |
| TP7 | PGND | Connected to PGND, the common for the input supply of the power stage, internally star-connected to GND |
| TP8 | IN+ | Connected to IN+ pin of the LMG1020, this is the positive logic input. |
Figure 9-2 Recommended Use for Ground Spring Clip Test Points
Figure 9-3 Visual and Description of Ground Spring Clip Test Points