SPAU024 April 2025 AM2612
The backward compatibility configuration is used for cases which require the controlSOM to interface to a AM26x controlCARD compatible baseboard or docking station. An HSEC adapter board (HSEC180ADAPEVM-AM2) is required for this configuration. Power is provided to the controlSOM through the HSEC Dock (TMDSHSECDOCK-AM263 or TMDSHSECDOCK). An emulation debug-probe such as the XDS110ISO-EVM is required to provide debug connectivity to the MCU. The HSEC adapter board, XDS110 debug probe, and HSEC dock are sold separately.
TMDSHSECDOCK-AM263 and TMDSHSECDOCK are baseboards that enable rapid prototyping and enhances the development capability of the AM261x controlSOM. The TMDSHSECDOCK-AM263 contains hardware to enable AM26x MCU-specific features that allow various peripherals not enabled onboard the controlSOM to be interfaced with. The TMDSHSECDOCK only enables access to the IOs pinned out to the SOM HD connectors. Table 2-2 compares the features of each docking station.
| Feature | TMDSHSECDOCK | TMDSHSECDOCK-AM263 |
|---|---|---|
| USB Type-C power input | ✓ | ✓ |
| GPIO breakout headers | ✓ | ✓ |
| Breadboard area for customizable routing and prototyping | ✓ | |
| 2-channel MCAN Transceiver | ✓ | |
| 2-channel LIN Transceiver | ✓ | |
| MIPI-60 debug header | ✓ | |
| 14-pin JTAG header | ✓ | ✓ |
| ADC input signal conditioning | ✓ |
In this configuration, Code Composer Studio connects to the controlSOM by JTAG and enables software development. The XDS110 debug-probe also enumerates a virtual COM port (VCP) for communication with the MCU by UART.
Follow these steps to enable this configuration:
Figure 2-2 AM26x controlCARD Backward
Compatibility Configuration - XDS110ISO Connected to HSEC180ADAPEVM-AM2 J4
Figure 2-3 AM26x controlCARD Backward
Compatibility Configuration - XDS110ISO connected to controlSOM J7