SPNU151W January 1998 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , OMAP-L132 , OMAP-L137 , OMAP-L138 , SM470R1B1M-HT , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Following are detailed descriptions of options that you will probably use frequently:
| --c_src_interlist | Invokes the interlist feature, which interweaves original C/C++ source with compiler-generated assembly language. The interlisted C statements may appear to be out of sequence. You can use the interlist feature with the optimizer by combining the --optimizer_interlist and --c_src_interlist options. See Section 3.11. The --c_src_interlist option can have a negative performance and/or code size impact. |
| --cmd_file=filename | Appends the contents of a
file to the option set. Use this option to avoid
limitations on command line length or C style
comments imposed by the operating system. Use a #
or ; at the beginning of a line in the command
file to include comments. You can add comments by
surrounded by /* and */. To specify options,
surround hyphens with quotation marks. For
example, "--"quiet. You can use the --cmd_file
option multiple times to specify multiple files.
For example, the following indicates file3 should
be compiled as source and file1 and file2 are
--cmd_file
files: |
| --compile_only | Suppresses the linker and overrides the --run_linker option, which specifies linking. The --compile_only option's short form is -c. Use this option when you have --run_linker specified in the TI_ARM_C_OPTION environment variable and you do not want to link. See Section 4.1.3. |
| --define=name[=def] | Predefines the constant name for the preprocessor.
This is equivalent to inserting #define name def at the top of each C source
file. If the optional[=def] is omitted, name is set to 1. This
option's short form is -D. If you want to define a quoted string and keep the quotation marks, do one of the following:
|
| --gen_func_info_listing | Generates a user information file with a .aux file extension. The file contains linker call graph information on a per-file level. |
| --help | Displays the syntax for invoking the compiler and lists available options. If the --help option is followed by another option or phrase, detailed information about the option or phrase is displayed. For example, to see information about debugging options use --help debug. |
| --include_path=directory | Adds directory to the list of directories that the
compiler searches for #include files. The --include_path option's short form is
-I. You can use this option several times to define several
directories; be sure to separate the --include_path options with spaces. If you do
not specify a directory name, the preprocessor ignores the --include_path option.
See Section 2.5.2.1. |
| --keep_asm | Retains the assembly language output from the compiler or assembly optimizer. Normally, the compiler deletes the output assembly language file after assembly is complete. This option's short form is -k. |
| --quiet | Suppresses banners and progress information from all the tools. Only source filenames and error messages are output. The --quiet option's short form is -q. |
| --run_linker | Runs the linker on the specified object files. The --run_linker option and its parameters follow all other options on the command line. All arguments that follow --run_linker are passed to the linker. The --run_linker option's short form is -z. See Section 4.1. |
| --skip_assembler | Compiles only. The specified source files are compiled but not assembled or linked. This option's short form is -n. This option overrides --run_linker. The output is assembly language output from the compiler. |
| --src_interlist | Invokes the interlist feature, which interweaves optimizer comments or C/C++ source with assembly source. If the optimizer is invoked (--opt_level=n option), optimizer comments are interlisted with the assembly language output of the compiler, which may rearrange code significantly. If the optimizer is not invoked, C/C++ source statements are interlisted with the assembly language output of the compiler, which allows you to inspect the code generated for each C/C++ statement. The --src_interlist option implies the --keep_asm option. The --src_interlist option's short form is -s. |
| --tool_version | Prints the version number for each tool in the compiler. No compiling occurs. |
| --undefine=name | Undefines the predefined constant name. This option overrides any --define options for the specified constant. The --undefine option's short form is -U. |
| --verbose | Displays progress information and toolset version while compiling. Resets the --quiet option. |