SPRABV4I October 2021 – August 2025 SM320F28335-EP , SM320F28335-HT , TMS320F280023-Q1 , TMS320F280025-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
The command line PC utility is a programming design that can easily be incorporated into scripting environments for applications such as production line programming. The command line PC utility was written using Microsoft Visual Studio® in C++. The project and the source can be found in C2000Ware (C2000Ware_x_xx_xx_xx > utilities > flash_programmers > serial_flash_programmer).
To use this tool to program the C2000 device, make sure that the target board has been reset and is currently in the SCI boot mode and connected to the PC COM port. The command line usage of the tool is described below:
serial_flash_programmer.exe –d <device> -k <kernel file> -a <app file> -p COM <num>
[-m] <kernel2 name> [-n] <app2 name> [-o] <kernel3 name> [-r] <app3 name> [-b] <baudrate> [-q] [-w] [-v] [-t]| -d <device> | The name of the device to connect and load to: F2802x, F2803x, F2805x, F2806x, F2807x, F2833x, F2837xD, F2837xS, F28004x, F2838x, F28002x, F28003x, F280013x, F280015x, F28P65x, F28P55x or F28E12x |
| -k <file> | The file name for the CPU1 flash kernel. This file must be in the ASCII SCI boot format. |
| -a <file> | The application file name to download or verify to CPU1 This file must be in the ASCII SCI boot format. |
| -m <file> | The file name for the CPU2 flash kernel. This file must be in the ASCII SCI boot format. |
| -n <file> | The application file name to download or verify to CPU2. This file must be in the ASCII SCI boot format. |
| -o <file> | The file name for the CM flash kernel. This file must be in the ASCII GPIO boot format. |
| -r <file> | The application file name to download or verify to CM. This file must be in the ASCII GPIO boot format. |
| -p COM<num> | Set the COM port to be used for communications |
| -b <num> | Set the baud rate for the COM port |
| -? or -h | Show help |
| -q | Quiet mode. Disable output to stdout |
| -w | Wait for a key press before exiting |
| -v | Enable verbose output |
| -t | This option is only applicable to the F28P55x device. The file name for the custom flash bank and sector erase configuration. Make this file in the format detailed in Specifying the Flash Banks and Sectors of the Application. |
-d, -k, -a, -p are mandatory parameters. If the baud rate is omitted, the baud rate is set to 9600 by default.