SPRABV4I October   2021  – August 2025 SM320F28335-EP , SM320F28335-HT , TMS320F280023-Q1 , TMS320F280025-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Programming Fundamentals
  6. 3ROM Bootloader
  7. 4Flash Kernel A
    1. 4.1 Implementation
      1. 4.1.1 Application Load
  8. 5Flash Kernel B
    1. 5.1 Implementation
      1. 5.1.1 Packet Format
      2. 5.1.2 CPU1 Kernel Commands
      3. 5.1.3 CPU2 Kernel Commands
      4. 5.1.4 Packet Data
      5. 5.1.5 Status Codes
    2. 5.2 F2838x SCI Flash Kernels
      1. 5.2.1 CPU1-CPU2 Kernels
        1. 5.2.1.1 Kernel Commands
      2. 5.2.2 CPU1-CM Kernels
        1. 5.2.2.1 Kernel Commands
      3. 5.2.3 Using the Projects With SCI Bootloader
        1. 5.2.3.1 CPU1-CPU2
        2. 5.2.3.2 CPU1-CM
      4. 5.2.4 Using the Projects With Code Composer Studio (CCS) Software
        1. 5.2.4.1 CPU1-CPU2
        2. 5.2.4.2 CPU1-CM
    3. 5.3 F28P65x SCI Flash Kernel
      1. 5.3.1 CPU1 Kernel
        1. 5.3.1.1 Host-Kernel Communication: ControlCard
        2. 5.3.1.2 Host-Kernel Communication: LaunchPad Development Kit
        3. 5.3.1.3 Kernel Commands
      2. 5.3.2 Using the Projects With SCI Bootloader
        1. 5.3.2.1 CPU1
      3. 5.3.3 Using the Projects With CCS
        1. 5.3.3.1 CPU1
    4. 5.4 F28P55x SCI Flash Kernel
      1. 5.4.1 Implementation
        1. 5.4.1.1 Specifying the Flash Banks and Sectors of the Application
      2. 5.4.2 Kernel
      3. 5.4.3 Using the Project With SCI Bootloader
      4. 5.4.4 Using the Project with CCS
  9. 6Example Implementation
    1. 6.1 Device Setup
      1. 6.1.1 Flash Kernels
      2. 6.1.2 Hardware
    2. 6.2 Host Application: serial_flash_programmer
      1. 6.2.1 Overview
      2. 6.2.2 Building and Running serial_flash_programmer Using Visual Studio
      3. 6.2.3 Running serial_flash_programmer for F2806x (Flash Kernel A)
      4. 6.2.4 Running serial_flash_programmer for F2837xD (Flash Kernel B)
    3. 6.3 Host Application: Firmware Updates on F28004x With SCI Flash Kernel
      1. 6.3.1 Overview
      2. 6.3.2 Boot Pin Configurations
      3. 6.3.3 Using Three Boot Modes
      4. 6.3.4 Performing Live Firmware Updates
  10. 7Troubleshooting
    1. 7.1 General
    2. 7.2 SCI Boot
    3. 7.3 F2837x
      1. 7.3.1 F2837xS
      2. 7.3.2 F2837xD
      3. 7.3.3 F2837xD LaunchPad™
    4. 7.4 F28P65x
  11. 8References
  12. 9Revision History

Implementation

Flash Kernel B is more robust than Kernel A. Flash Kernel B communicates with the host PC application provided in C2000Ware (C2000Ware_x_xx_xx_xx > utilities > flash_programmers > serial_flash_programmer) and provides feedback to the host on the receiving of packets and completion of commands given to it.

After loading the kernel into RAM and executing the program through the SCI ROM bootloader, the kernel first initializes the PLLs of the device, initializes SCIA, and takes control of the flash pump, if necessary. The program then waits for an 'a' or ‘A’ from the host to perform an auto baud lock with the host. After this, the kernel begins a while loop, which waits on commands from the host, executes the commands, and sends a status packet back to the host. This while loop breaks when a Run or Reset command is sent.

Commands are sent in a packet described in Table 5-1 and each packet is either acknowledged or not-acknowledged. All commands, except for Run and Reset, send a packet after completion with the status of the operation. The status packet sends a 16-bit status code and 32-bit address. In case of an error, the address in the data specifies the address of the first error. In case of NO_COMMAND_ERROR, the address is 0x12345678.

In the case of a Device Firmware Upgrade (DFU) command, the following steps take place:

Note: These steps do not apply to F28P55x. For details on the F28P55x device, see F28P55x SCI Flash Kernel.
  1. The kernel receives a file in the hex boot format byte-by-byte from the SCI module and calculates a checksum over the block size. After receiving the block of data, the kernel sends back the checksum.
  2. After receiving a block of data and storing it in a buffer, the kernel erases the sector if it has not been previously erased, and programs the data into flash at the correct address along with ECC using the flash API library.
    Note: To get more information on the blocks of data and how block size is determined, see the Bootloader Data Stream Structure section of the device-specific TRM. Note that the block and block size mentioned here are not to be confused with the command packet mentioned earlier.
  3. Afterwards, the kernel verifies that the data and ECC were programmed correctly into flash.
    Note: This kernel only erases sectors that are needed to program the application and data into flash. This is different from Flash Kernel A that erases the entire flash at the start of kernel execution. However, Flash Kernel B also supports an erase command independent of the DFU command, which gives the user the ability to erase specific sectors or the entire flash of the device.

Similarly, the verify command receives a file in the hex boot format and in place of erasing and programming the flash, the kernel only verifies the contents of the flash.