SPRACT9A September   2020  – May 2024 AM6526 , AM6528 , AM6546 , AM6548 , AM68 , AM68A , AM69 , AM69A , DRA821U , DRA821U-Q1 , DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VM , TDA4VM-Q1 , TDA4VP-Q1 , TDA4VPE-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Tuning Algorithm Overview
  5. 2Hardware Tuning Algorithm
  6. 3SW Tuning Algorithm
  7. 4Revision History

SW Tuning Algorithm

For software tuning, everything that would have been done automatically by the hardware module is now enabled via software coding. The software program will sequence through all 32 delay ratio elements, issue CMD19/CMD21 and record the pass and fail results at each ratio element. Then, the program will find the optimal delay ratio element for functionality use. Figure 3-1 describes the process in detail.

 MMC SW Tuning Algorithm Figure 3-1 MMC SW Tuning Algorithm

If DLL is used (ENDLL = ‘1’), then the 32 ratio elements will constitute a whole clock cycle. Delaying the CLK by Ratio 32 will mean delaying the CLK by Ratio 0. As a result, the biggest passing window should be taken as the window that wrapped around from the end to the beginning of the delays. If DLL is not used (ENDLL = ‘0’), the biggest passing window should be taken as the window without the wraparound applied.

 Setup Hold Time
                Requirements Figure 3-2 Setup Hold Time Requirements
 Selection of Tuning Ratio for
                Functionality With DLL Enabled Figure 3-3 Selection of Tuning Ratio for Functionality With DLL Enabled

As a safety precaution, software code should also implement a re-tuning mechanism to re-tune the delay module if the MMC functionality fails. This can be done by checking for data line status bits for errors. If errors occurred, re-execute the tuning sequence. Re-tuning should also be done at timer expiration by using the re-tuning functionality.

Note:

Uncommon Data Error During Tuning

Note that during software tuning there can be a few uncommon data errors, such as data or cmd line being reset. These data errors that happen during software tuning should be ignored by the driver because these errors are expected while tuning.