SPRADB3A October 2023 – November 2024 AM2612 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
AM261 comes with two changes to the memory module. The first is an increase in available Tightly-Coupled Memory (TCM) from 128kB to 256kB per CPU core. The second is a reduction in the total on-chip RAM (SRAM) where AM263P offers 2MB to 3MB of SRAM while AM261 offers 1MB to 1.5MB of SRAM. The amount of SRAM present depends on device variants. Details on the specific memory sizes per device variants can be found within the respective device datasheets under the Operating Performance Points section.