SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
The ERRORSTS pin is an ‘always output’ pin and remains low until an error is detected inside the chip. On an error, the ERRORSTS pin goes high until the corresponding internal error status flag for that error source is cleared. Figure 3-4 shows the functionality of the ERRORSTS pin.
The ERRORSTS pin is tri-stated until the chip power rails ramp up to the lower operational limit. As the ERRORSTS pin is an active-high pin, users who care about the state of this pin during power-up must connect an external pull-down on this pin.
Figure 3-4 ERRORSTS Pin Diagram