SPRUHW1A June 2014 – October 2021 TMS320F28052-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28054-Q1 , TMS320F28054M , TMS320F28054M-Q1
InstaSPIN-MOTION is designed in a modular structure. Customers can determine which functions will be included in their system. The FAST Observer resides in ROM. The core control algorithms of the SpinTAC library reside in ROM, and these functions are accessed by Application Program Interface (API) from the user code.
InstaSPIN-MOTION supports a wide array of system designs. InstaSPIN-MOTION uses the FAST software encoder for sensorless FOC systems (for additional information, see the TMS320F28052F, TMS320F28054F InstaSPIN-FOC™ Software Technical Reference Manual). InstaSPIN-MOTION also supports solutions that leverage mechanical sensors (for example, encoders and resolvers). These scenarios are described below.
The variables in Figure 4-1, Figure 4-2, Figure 4-3, and Figure 4-4 are defined as:
: acceleration limit
: jerk limit
: acceleration reference
: motor time constant