SPRUIT8D February 2020 – February 2021 AWR2243
The AWR2243BOOST contains a SPI/CAN selector switch (S1) shown in Figure 2-14. However, the AWR2243 does not support CAN communication, so this switch should always be set to the ‘SPI’ position to bring out the SPI interface to the HD connector (J1). For more details on the HD connector,refer to Section 2.4.2.
Figure 2-14 S1 Switch to Select Between SPI or CAN Interface