DCC has provision to read the counts during operation. This is performed using DCCCNT0, DCCVALID0DCC_CNT0DCCCNT0DCC_VALID0DCCVALID0, and DCC_CNT1DCCCNT1 DCCCNT1 registers. Read from these registers in default mode allows reading the present value of count. This is useful when in single shot mode or mode where DCC stops upon error.
These registers can be used to read the FIFO through the DCC_GCTRL2[7-4] FIFO_READ
configuration. Reads on the empty FIFO shall provide the contents of last pointed location.
Application shall track the empty/full conditions of the FIFOs to track the count records
consistently.
Regardless of FIFO_READ configuration, the FIFO internally keeps updating records based on configured triggers until full.
Note:
- Input0_clk and input1_clk are two asynchronous clock domains. In a system, VBUS clock
may also be asynchronous relative to both Input0_clk and Input1_clk. The module must be
able to generate an error when either Input0_clk or Input1_clk is not present. VBUS
clock should not sample or affect the clock counting logic in any way.
- In general, the reference clock should be hooked up to Input0_clk and measured clock
should be connected to Input1_clk. The default clock source i.e. ‘0’ should be assigned
to connect with device native clock such as internal oscillator reference on both.
- The error interrupt signal is independent of the error flag bit. If the interrupt is
masked, the error flag is still set when an error occurs. The error flag stays set until
it is cleared, regardless of the status of the interrupt.
- The done flag in the DCCSTAT register would be set when the single shot mode completes
without error and is independent of the DONEENA bits in the DCCGCTRL register. The done
level interrupt would be set only if it is enabled by the DONEENA bits.
- Upon debug access, the FIFO pointers do not advance, hence not impacting the
functional behavior.