SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Table 30-47 lists the memory-mapped registers for the AES_SS_REGS registers. All register offset addresses not listed in Table 30-47 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
4h | AES_GLB_INT_FLG | AES Global Interrupt Flag Register | Go | |
8h | AES_GLB_INT_CLR | AES Global Interrupt Clear Register | Go |
Complex bit access types are encoded to fit into small table cells. Table 30-48 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
W1C | W 1C | Write 1 to clear |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
AES_GLB_INT_FLG is shown in Figure 30-52 and described in Table 30-49.
Return to the Summary Table.
The AES_GLB_INT_FLG register contains the current status of the AES interrupt
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | INT_FLG | ||||||
R-0h | R-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | RESERVED | R | 0h | Reserved |
0 | INT_FLG | R | 0h | Global Interrupt Flag for AES INT. This bit determines whether the SINTREQUEST is generated by AES This bit can be cleared by writing a 1 to the corresponding bit in the AES_GLB_INT_CLR register. Reset type: SYSRSn |
AES_GLB_INT_CLR is shown in Figure 30-53 and described in Table 30-50.
Return to the Summary Table.
The AES_GLB_INT_CLR register is used to clear the interrupt flags in AES_GLB_INT_FLG register.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | INT_FLG_CLR | ||||||
R-0h | R/W1C-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | RESERVED | R | 0h | Reserved |
0 | INT_FLG_CLR | R/W1C | 0h | Global Interrupt flag clear for AES INT. This bit is used to clear the corresponding bit in the AES_GLB_INT_FLG register. Write 1 to clear the INT_FLG bit. Writing 0 has no effect. Reset type: SYSRSn |