SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
There are independent data memory blocks. The behavior of the data memory depends on the state of the MMEMCFG[RAM0E] MMEMCFG[RAM1E] bits. These bits determine whether the memory blocks are mapped to CLA space or CPU space.
In this case the memory block is mapped to the CPU.
Priority of accesses are (highest priority first):
In this case the memory block is mapped to CLA space. The CPU can make only debug accesses.
Priority of accesses are (highest priority first):