SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Message RAMs consist of four blocks:
These blocks are useful for passing data between the CLA and CPU or CLA and DMA. No opcode fetches, from either the CLA or CPU, are allowed from the message RAMs. A write protection violation is not generated if the CLA attempts to write to the CPU to CLA or DMA to CLA message RAM, but the write is ignored. The arbitration scheme for the message RAMs are the same as those for the shared memories, described in the Memory Controller Module section of the System Control and Interrupts chapter.
The message RAMs have the following characteristics:
The following accesses are ignored:
The following accesses are ignored: