SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
Figure 28-25 shows how the interrupt mechanism works in the eQEP module.
Figure 28-25 eQEP Interrupt Generation
Eleven interrupt events (PCE, PHE, QDC, WTO, PCU, PCO, PCR, PCM, SEL, IEL, and UTO) can be generated. The interrupt control register (QEINT) is used to enable/disable individual interrupt event sources. The interrupt flag register (QFLG) indicates if any interrupt event has been latched and contains the global interrupt flag bit (INT).
A pulse interrupt is generated to the Interrupt Controller when the following conditions are met: