SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
FILE: ecap_ex1_apwm.c
This program sets up the eCAP module in APWM mode. The PWM waveform will come out on GPIO5. The frequency of PWM is configured to vary between 10Hz and 20Hz using the shadow registers to load the next period/compare values.